Utilities are beginning to transition away from natural gas to become more sustainable. They understand that in the long term, exploration, drilling and production of natural gas aren’t friendly to the environment. That’s why Honeywell’s standard gas meters can support the use of hydrogen, including the first-ever commercially available 100% hydrogen-ready diaphragm gas meter.
The hydrogen economy is moving fast to meet some of the world’s most ambitious goals. And this is just another step to getting future-ready. These meters are all capable of efficiently measuring hydrogen and can be connected to the existing infrastructure, saving time and money with this easy carbon-friendly transition.
The Hydrogen Economy Is Coming Fast. Are You Ready?
Honeywell has the first-ever commercially available 100% hydrogen-ready diaphragm gas meter. It provides unparalleled accuracy while still using the utilities’ existing infrastructure. So, get ready for the future. Honeywell shows you how it’s done.