/content/pmt/us/en/search-results.html

Honeywell Spectra® Medical Grade Fiber Awarded ISO 13485 Certification

Honeywell Spectra® Medical Grade Fiber Awarded ISO 13485 Certification

Ultra-lightweight and ultra-high strength fiber earns industry management standard recognizing safety and quality.

MORRIS PLAINS, N.J.  – Honeywell today announced its Spectra Medical Grade (MG) fiber has received ISO 13485 certification for manufacturing to supply the medical device industry.

ISO 13485, the highest management standard for the medical device industry, specifies requirements for a quality management system (QMS) where an organization needs to demonstrate its ability to provide medical devices and related services that consistently meet customer and applicable regulatory requirements.

Spectra MG, an ultra-lightweight and ultra-high strength fiber, is incorporated into the design of medical devices used in minimally invasive procedures. It gives medical device manufacturers greater flexibility to design and build smaller, stronger and lighter devices.

The ISO 13485 certification will allow Honeywell to implement a medical device quality management system to identify, manage and minimize the risks involved with the manufacturing and sale of raw materials and components for medical devices. The certification will improve processes and ensure quality consistency by defining requirements and standards that meet medical device industry requirements.

“As regulations become more stringent, this certification is critical for our customers and will help them manage their risk and help enable regulatory approval of their devices,” said Abey Paul, business leader for Spectra MG Fiber, at Honeywell. “With Spectra MG, medical device manufacturers can continue to develop and bring to market smaller and more effective devices that are stronger and lighter in weight.”

The certification will also enable cost reductions of non-conforming products for customers, and help them meet the objective standard of excellence to enhance their competitive advantage in the marketplace.

Compared with conventional polyethylene fiber, Spectra MG has an ultra-high molecular weight, high degree of orientation, and crystallinity, that leads to higher fiber strength and better wear resistance to surface damage. It is three times stronger than polyester in a volume basis and is highly resistant to chemicals, water and ultraviolet light.  Spectra MG fiber’s high resistance to chemicals, fatigue and abrasion and low friction for easier movement, makes it a suitable biomaterial for many applications in the medical device industry.

Honeywell (www.honeywell.com) is a Fortune 100 technology company that delivers industry specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help everything from aircraft, buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable.  For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

ISO (International Organization for Standardization) (www.iso.org) is an independent, non-governmental international organization with a membership of 165 national standards bodies. ISO 13485:2016 is the standard for a Quality Management System (“QMS”) for the design and manufacture of Medical Devices.

Stephanie Agresti
Sr. External Comms Specialist